This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561-R2: CHEMID for LTO single cell battery

Part Number: BQ27Z561-R2
Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO

Hello,

Our customer wanted to use this device with a Lithium Titanate Oxide single-cell battery. They have followed the instructions for capturing a log file using bqStudio and have sent the log file to GPCCHEM website.  However, the result of the submission was that a suitable CHEMID could not be found.

Would you kindly help on how to get a suitable CHEMID for this battery?

Please refer to the battery details and log files provided by the customer below:

The nominal voltage of the LTO is 2.4V, the full charge voltage is around 2.8V and the discharged voltage is approximately 2.2V

GPCPackaged (1).zip

Thank you.

Regards,

Marvin A.