Hello,
We are working with the UCC256404 and trying to calculate burst mode values.
From the datasheet, we came up with the values for Rll/ss1 as 390k and Rll/ss2 as 180k. We are using Option 6 to determine the ratio of BMTl:BMTh by selecting proper BW pin resistors.
Based on those 2 resistors, we are getting burst threshold voltage of Vbmt_h = 0.491V and Vbmt_l = 0.295V.
Our question is what Rll/ss3 resistor should we select to make sure the converter only goes to burst mode when PFC_ON is disabled. Is there any calculation we can use to do that ?
Thank you, Keith