Good Morning,
I built the circuit on page 5 of this manual:
http://focus.ti.com/lit/ug/sluu023b/sluu023b.pdf
except I left resistors R15, R16, and R17 out because I don't think I needed them based on my application. I also used slightly different resistor values for R3 and R2 due to the thermistor that I was using. I also included an analog ammeter between L1 and BAT+ and an analog voltmeter across BAT+ and BAT-. The voltmeter seems to be interfering with the TI pre-qualification test and it never gets to the battery absent standby mode if no battery is present. I notice that it doesn't do this with a digital voltmeter across BAT+ and BAT-. I am not an electrical engineer so I don't really have the background to troubleshoot this problem. I can only assume that the current through the analog voltmeter is sufficient to trick the BQ2031 into thinking that a battery is connected. Can anyone suggest a workaround for this or suggest another reason why this may be happening?
Thanks
Saleem