Dear TI Team,
What will be the limitation to select Fmin.
In the datasheet application note 300W , Fmin selected as 45KHz. and Calculated Inductor Value =340uH.
1. Is it possible to increase Fmin to 100Khz and Calculate the Inductor , because designing the Inductor with Low switching frequency , size will be increase.
2. If I increased the Frequency to 100Khz for my application then the calculated Inductor = 94uH and the RT resistor value is coming 29.53Kohm from the equation and as per the recommended value TSET resistor =( 66.5 to 270Kohm), since resistor value 29.53k ohm < 66.5kohm , as per my understanding I can not go with 100KHz frequency (please confirm)
3.It means the Fmin value is limited by the recommended by TSET resistor (66.5kohm to 270Kohm). (please confirm)
4.During the Inductor Design shall we go for 1/2 Inductor value of calculated inductor . (please confirm)
Thank you.
Regards,
Sachin Khante