This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82866A: tdelay

Part Number: TPSM82866A

Hi team,

Could you please help with following question?

there is a description ''The tDelay time varies with the VSET/MODE resistor used and is longest with a resistance of 249 k or higher''

And there is a table as following:

so I am little confusing here, for example, I am wanting a 0.90V output, I should choose a 18.7k resistor at Vset/mode pin.

Q1. Will my tdelay to be a matched delay time, right?

Q2. if Q1 answer is 'Yes', so there will be only one delay time under one output voltage condition, this delay is not actually adjustable?

Q3. How about, if Vset pin is 0.90V, the Vset/mode logic is low, so the part must worked under a PSM?

Thanks

Best regards

Mia Ma