Other Parts Discussed in Thread: BQSTUDIO,
Hi,
I have many question about to calculate Balance Time per mAh and value of Bal Time/mAh Cell-1 config in BQStudio.
I will make External Cell Balancing in my system.In Technical Reference Manual document of BQ40Z80, recommended that formula to Balance Time per mAh Cell 1 and Cell 2-7.I will share my parameters and calculation to calculate Bal Time/mAh Cell1, Bal Time/mAh Cell 2-7.
VCELL = 3200mV
RVCx = 200 ohm
Rcb = Fet on Rds = 25 mOhm
DUTY = cell balancing duty cycle %75 typ. I used the typical value.Should I use that value?
Rext = 30 ohm
According to formulas,
Balance Time per mAh Cell 1 = 39 s/mAh
Balance Time per mAh Cell 2-7 = 32 s/mAh
I will fill in the values which I calculated above to BQStudio Advanced Charge Algorithm Cell Balancing Config section?
Can you check the my calculations?
Thank you.
Sincerely.