This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: Max Charge Current =32767mA in lifetime , External 2 Temperature=3003.5℃ in PF Status

Part Number: BQ28Z610-R1
Other Parts Discussed in Thread: BQSTUDIO

Hello,

I have a battery pack cannot be charged. and I find PF=1 in Operation status, CFETF=1 in PF status C+D at Bit registers. 

And also find Max Charge Current =32767mA in lifetime , External 2 Temperature=3003.5℃ in PF Status at Datamemory. these big data in red background color can tell us what? Is there something wrong with Gauge IC?