This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170: nFAULT pin output condition

Part Number: LM5170
Other Parts Discussed in Thread: LM5171,

Hi Experts,

I would like to confirm the condition when nFAULT pin outputs low. For my customer's use-case, since the circuit barker is not required, SYNCOUT pin is pulled low with 10K ohm resister. In this scenario, nFAULT pin output has no meaning meaning never drive low output. Is this understanding correct?

Also, when SYNCOUT pin is left to open, nFAULT can be used to detect the short between source and drain of FET before stating up. Even if other fault conditions like overvoltage, overcurrent and thermal shutdown occur, nFAULT pin does not drive low. Is this understanding correct?

Regards,

Uchikoshi