This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256403: About the timing to apply VCC

Part Number: UCC256403
Other Parts Discussed in Thread: UCC28180,

Hello,

I am considering using UCC256403(LLC) and UCC28180(PFC).
I would like to ask you about when to apply the VCC of UCC256403 at startup.
In order to avoid overlapping the timing of the inrush currents of PFC and LLC at startup, we plan to start LLC after the output voltage of PFC is completely stable.
In this case, as the operation of LLC, it is assumed that 13V is applied to VCC after the voltage of the BLK pin exceeds the start threshold value for a while.
This state is when the BLK voltage reaches the BLKStart level before the VCCStartSwitching threshold is exceeded.
Is this behavior possible?

Best regards,