This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256403: Can I connect the VCC pin and RVCC pin?

Part Number: UCC256403


Hello,

UCC256403 is used, but 13V will be applied to VCC from the outside.
At this time, is it okay to connect the VCC pin and RVCC pin to eliminate the loss of the internal LDO?

Best regards,