This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54200: reference voltage when PWM is pulled high

Part Number: TPS54200

Hi team,

In customer's design, PWM is pulled high by MCU GPIO default high status. In this status, is the reference voltage 100mV or 200mV?

Thanks.

  • Hi Jerry,

    Once tps54200 is enabled, after 30us, the device will decide to choose analog dimming or PWM dimming. if the external is higher than 2.07V, analog dimming is chosen while PWM dimming is selected when external signal is between 1V and 2.07V.

    So come back to your question, if the GPIO's voltage is higher than 2.07V when tps54200 is enabled for the first time. then FB voltage is 200mV(analog dimming mode). Once the dimming mode is selected, it's locked and will not change whatever GPIO's voltage is unless tps54200 is enabled again.

    Robin