Part Number: BQ77PL900
Hi team,
Here's an issue from the customer may need your help:
The customer used BQ77PL900 to connect 8 groups of tandem lithium-polymer.Each battery pack has 5 pieces of lithium-polymer in parallel .Each battery voltage 4.2V. The designed board can work normally.
Now they are going to replace lithium-polymer with Li-Lion of the same voltage . Use This board to Connect 8 groups of tandem Li-Lion.Each battery pack has 6 pieces of Li-Lion in parallel. However, after the Li-Lion battery pack is connected to the board, overvoltage is displayed . Is there any difference between LI-lion and li-polymer for BQ77PL900 that should be noticed?
Could you help check this case? Thanks.
Best Regards,
Cherry