Hi , I have an audio amplifier(http://focus.ti.com/lit/ds/slos516c/slos516c.pdf) which requires a supply of 10 to 26 V , and in my system I have micro controller which needs 2.6 to 3.6v. i'm facing problem at the selection of power source to this audio amplifier and controller Hence I have selected two TPS5410 one from 20 v to 18 v, 1 A(for audio amp) and other one is for controller(20 to 3 v , 1A) , will this do the help ..? source to the TPS5410 is from 20v ac to dc adaptor ... regards chethan