This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25892: - Can this be used as a standalone charger?

Part Number: BQ25892
Other Parts Discussed in Thread: BQ25616, BQ24170, BQ24172

The design I'm working on will need standalone.

I haven't got this IC to supply any current, and the datasheet shows I2C connections on each of the application examples. It seems to be I2C control mainly

The requirements are 4A or more, nominal voltage 3.65V, charging voltage 4.2V, lithium ion, input voltage 5V ideally, variable charge current ideally also (2A and 4A switchable)

Thank you in advance for any assistance