Hi. I'm using an LM3409 MOSFET driver to drive a LED. Apparently, it seems like there are spikes occurring when I make a sweep from lower V_IADJ values to a higher value (see picture 1). These "spikes" occur in different parts of the sweep every time I run a test. It seems like the spikes on this sweep have an offset from the expected true value of about 2.5% but I have seen spikes where the spike offset is about 20%. I have monitored the V_IADJ voltage and nothing seems to be wrong on that end (see picture 2). On Picture 2 I made another test where the A_IADJ has the same voltage for all exposures. Here it's clear that the average output is higher on the first exposure and lower on the second even though the V_IADJ has the same voltage. (The spike at the end is not a problem. It is only the average current that is the problem)
Is this something you can explain or have experienced before?
Picture 1.
On
Picture 2.