Hi,
I want to design a circuit ,that is capable of applying either a 28V or 0V across a semiconductor device.The circuit should be capable of sourcing(while 28V across load) & sinking(while 0V across load) around 200mA.
So i was considering a MOSFET based solution, will a complementary pair of MOSFETs can be used for this application?If so does there exists any suitable simple gate drive circuit or chip to use with?
Thanks& Regards
Stephen