Other Parts Discussed in Thread: TPS61041,
Hi Expert,
This is Koki Tsushima.
My customer will evaluate EVM of TPS61096A, but wants to know why this efficiency lower than TPS61041 at Vout 12V, Iout 1mA ?
As fig.1 that efficiency is around for 80%.
It seems to be lower than TPS61041 (Although some condition is different).
Could you tell me the reason why this is low and just around 80%?
Customer think this is due to 2ch level shifter was powered by Vout, but this consumption is just 3uA, therefore, it should not be correct.
In addition, customer want to use for light load.
If customer ignore efficiency than 100mA, do you have ideas which can improve the efficiency more for less than 100mA?
Best regards,
Koki Tsushima