This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: Power management forum

Part Number: LM7480-Q1


Hi,

Discovered an issue when evaluating LM74801 which is configured as Common source config with cut off mode.

Noticed that with a pulse of 30V (100ms pulse) on top of 13V, causes no output of the LM74801  after the pulse back to 13V. Found that the Hgate kept oscillating and didnt turn on as expected.

However no similar issue observed with  30Vpulse with 70ms duration on top of 13V.

Repeating the test with Vin of 20V (100ms pulse) on top of 13V, observed that the LM74801 had some oscillation  on Hgate before it recovered.

Would like to have private chat before posting any scope shot and schematic.