This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31710: For this material, do we have the replacement material in stock?

Part Number: LMZ31710
Other Parts Discussed in Thread: LMZ31707

  • For this material, do we have the replacement material in stock?

  • Hi Xiaofu,

    TPS84A20RVQT is 100% compatible with LMZ31710, and can replace LMZ31710.

    If you do not need the 10 A current at the output you may want to consider  LMZ31707 (7 Amps output) or LM31704 (4 Amp output) as well.

    I have not checked the availability of any of these in the stock. You can look for availability at ti.com.

    Regards,

    Yitzhak Bolurian