Part Number: TPS65145
Hello
I am using TPS65145 with output current of 25mA. per TPS65145 datasheet figure 12, the efficiency is ~72%.
Reading in the datasheet page 13 section 8.2.2.1.1 it is stated that the efficiency is inductor dependent. The dependency is influenced by:
- DCR dependent: The lower the DCR. The better the efficiency.
- Form Factor dependent: The larger the form factors the better the efficiency (2% to 10%).
but, looking at Table 2 (page 14) - "Inductor Selection".... looking at 3.3uH inductors and arrange them by form factor...smaller to higher:
3.3 µH Sumida CDRH2D18/HP 3R3 3.2 × 3.2 × 2 1.45 A, 69 mΩ
3.3 µH Sumida CDPH4D19 3R3 5.1 × 5.1 × 2 1.5 A, 26 mΩ
3.3 µH Coilcraft DO1606T-332 6.5 × 5.2 × 2 1.4 A, 120 mΩ
3.3 µH Coilcraft LPO6610-332M 6.6 × 5.5 × 1 1.3 A, 160 mΩ
The DCR is not reduced with a larger form factor as written in the datasheet.
Can you explain why? Is it because of different inductor material?