This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792EVM: BQ25792EVM

Part Number: BQ25792EVM


There is no S1 on the USAB2ANY box!

  • Hi Ramin,

    From the user's guide at 

    S1 is inside the case beside the USB Mini-B port.  You need to use a small still rod like a leaded resistor or mechanical pencil to press it.\

    Regards,

    Jeff

  • Thank you. I fixed this issue.

    I am powering the EVM board using external power supply +24VDC @5A

    Once I connect the uUSB connection from EVB to the PC, the PC turns off!

    Which Jumper(s) to remove or change it position on the EVM board?

    Thank you

  • HI Ramin,

    You either use the USB port, connected to VBUS, D+/D- and GND pins of the charger so the PC's port can power the charger, OR you can connect to an external supply.  In your config, you are shorting a 24V power supply to the PC's USB 5V output, which is causing the PC to protect itself.

    Regards,

    Jeff