This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74670-Q1: Alternate part for LM74670 which Can support up to 400KHz Operation

Part Number: LM74670-Q1

Hello Experts,

I am designing an AC to DC rectifier for <40V. The LM74670-Q1 supports operation only till 300HZ. But, My application needs 350KHz. Are there any other parts similar to this which Can support the higher frequency range?

Regards

Vishal

  • Hi Vishal,

    LM74670-Q1 is an Ideal diode controller which offers input reverse polarity protection. This device can also be used for low Frequency AC- Rectification upto 300 Hz. This device or any of the devices in the same family were not designed for high frequency operation as high as 350 kHz.

    May I know your AC-DC architecture, so that I can direct this query to the right contact who can help you choose the best controller for your design.

  • Hi Praveen,

    Thanks for your response. In my application, Input is a sine wave of amplitude up to 42V and 350KHz. I need to convert this to DC (same like AC to DC bridge rectifier. I don't want to use Schottky diodes. So looking for active bridge drivers like LM74670.

  • Hi Vishal,

    Unfortunately for bridge rectifier architecture, we do not have any device/controller similar to LM74670-Q1 which can rectify a 350KHz sine wave.