Dear experts
We have facing an condition that the device often got into the Safe recovery. So there have some condition need to have a confirm.
1. How long the time interval is when the device have a error to add the recovery counter?
2. If the device continue over temperature, or continue UV, how much time it takes to add the recovery counter from 0 to 15?
3. If the error removed, the device will have BOOT BIST test, some time we are facing LBIST and ABIST error, but there do not have too much details about which kind of parameters have been checked, so is there some more details about the BIST test parameters?
Thanks
Jun Shen