Hey team,
I have a few questions regarding the TPS61665 which will be driving 16V @ 40mA max current. The LEDs are comprised of 2 parallel strings of 5 LEDs (Vf=3.2V) w/ 20mA passing through each string. They need to be able to dim the backlight leds.
Their PWM output is a 3.3V level signal at 133Hz, not the 1.8V signal in the circuit above. The dimming is changed by the modulation of the PWM duty cycle.
1. Can this part be used with a 3.3V drive at 133Hz
2. If so, what would that circuit topology look like
3. What would be the performance tradeoffs? (Noise / efficiency / etc),
Additional questions:
- What is the "d" shown in figure 16 of the datasheet in the equation for LED current?
- Are there any simulation tools for this device?
- I see there is a transient p-spice model
Thanks,
Cameron