Other Parts Discussed in Thread: LM51501-Q1, , TPS61023, LMR61428
Hello,
I have a very similar query to an old post which is linked here.
My requirements are for a boost converter that provides up to 400mA at 6V. The minimum input voltage should be 1.8V and the max input 3.1V. I'll be using a CR2 Lithium Battery.
The WeBench suggests the LM51501-Q1 however I'm not sure that this is ideal for use in a non-automotive application? My solution should prioritise low Iq and small physical size.
The linked post for LM2623 suggests it could be suitable but I understand it's quite an old chip. Are there any other TI chips that are more suitable for my requirements?
Thanks,
Tom