This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92513: Can TPS92513 control the constant output current with 3mA~600mA range by PDIM signal on duty?

Part Number: TPS92513


One of my customers is considering using TPS92513.

At this moment, they have the following question.
Could you please give me your reply?

Q. We want to control the constant output current with 3mA~600mA range by PDIM signal on duty (PDIM frequency = 250Hz)?
    Can TPS92513 control it without any problem?

Your reply would be much appreciated.

Best regards,

Kazuya.