Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM, EV2400, , BQ40Z50, BQEVSW
Hi! I'm currently working on a project where I need to use a Battery Management System with an MCU. I am wondering if it is possible to send commands through SMBus with the MCU through to the BMS, for purposes such as changing the ChemID, setting the device to different modes, etc. Is it possible to do this without the BQStudio and the evaluation boards?
With regards to ChemID - I will be using a Li-Ion battery to support the project. I've read in a couple of threads that these devices come pre-loaded with firmware and default settings. I've also read that ChemID is a proprietary feature locked by Texas Instruments, and thus (at least from what I have visibly seen on this forum), they are uneditable - although perhaps there are 'other' ways. I am wondering if the type of battery is the only important property of the ChemID, and if the BQ-device comes preloaded with Li-Ion as its default setting. If the situation is so that I must edit the ChemID, how should I approach this problem?
And finally, can the BQ-device be used right away after setup and providing the necessary power supplies?
Best,
Riz