Other Parts Discussed in Thread: LM317, TPS7A85, TPS7A4001, TPS7A94, TPS7A57
Hi LDO team,
I wonder how fast LM317HV can respond to the variation of R2. Customer tries to adjust the voltage of ADJUST pin to vary the output voltage. (like figure 12 in LM317 datasheet)

1) I believe I can check the BW of LDO as a point of reference when it comes to the transient response time. Are the BW of LM317HV and LM317 same?
2) May I know the bandwidth of LM317(HV)?
3) I notice LM317 has a different structure from other LDO that I'm familiar with - TPS7A85, TPS7A4001, etc.. It look LM317 has an unity gain structure that output node is directly connected to negative node of internal OPAMP. Is this structure has any advantage when it comes to the transient response time?
<LM317 internal structure>

<TPS7A4001 internal structure>

It would be appreciated if you can provide more advice on the difference between two products - LM317 (which is unity gain structure) and TPS7A4001 (which is not) - and on which parameters I should look at in order to check the response time of LDO.
Thank you.