This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

4S Lithium ion charger *and* balancer IC



So, I need a stand alone switch mode IC to manage/charge a 4 series lithium ion battery pack.  But all the ICs I see charge from either end of the battery pack only.  So rather than simply placing 4.2x4=16.8V across my 4S pack (as the final charging stage) I need to also ensure that each cell has no more than 4.2V across it - that is balance the pack.

Any ideas on a suitable IC?  Thanks.