Hi,
I understand the TPS62203 device requires an input voltage of 3.6V to 6V to generate a regulated output voltage of 3.3V with an output current between 0 and 300mA.
With an input voltage between 2.5V and 3.6V what will be the output voltage for this device e.g.
If Vin = 2.7V and Iout = 1mA to 50mA, will the PMOS pass transistor be switched fully on for this example, so Vout = Vin i.e. 2.7V?