Other Parts Discussed in Thread: LM2621, LMR61428
Hello,
I was hoping I could get some help choosing the right TI part. I need a boost converter for a 2cell AA battery application.
Vin min = 1.8
Vin max = 3.1
Vout = 8V
Iout max = 200mA continuous
Ambient temp max = 35 deg C
I was looking at the LM2623A, which seems like it can achieve this and it seems to be available to purchase at higher quantity right now, which is a difficult task these days. But wanted to see what other options TI has. I tried Web bench tool, but that didn't really turn up any results.
If LM2623A is the best option, I had a question about the Vdd pin.
- The datasheet says the Vdd pin can have a maximum of 10V, but the recommended operating conditions say 5V max. Can I power Vdd with my 8V output? I don't see any application notes with example circuits with Vout higher than 5V. Or will I have to regulate by 8V down to 5 to power Vdd?