This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54140:It outputs -15V with 15V input, but it does not start up according to the design value of soft start.

Part Number: TPS54140


Hello.
We become indebted to.
I am using your TPS54140 with a 15V input and an output of -15V. 
However, I set the soft start to 3.2ms, but it started up in 200ms.
I want to start up to -15V in about 3.2ms, is there a solution?
Please refer to the waveform below.