This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28051: 400W PFC capability

Part Number: UCC28051
Other Parts Discussed in Thread: UCC28063, UCC28180, UCC28019A

Hi Team,

UCC28051 is  transition mode pfc controller and datasheet "8.2.1 Design Requirements" output power is 100W.

My customer output power requirement is 400W but can UCC28051 or UCCx805x support 400W capability?

I read below e2e and 700W capability is discussed but not 400W capability.

(+) PFC device for 400W and 700W output - Power management forum - Power management - TI E2E support forums

Regards,

Kai

  • Hello Kai,

    The power is handled by the power devices outside of the controller so the controller itself doesn't have a maximum power level it can support.  Generally speaking however, with single phase TM PFC controllers (sometimes referred to as CRM) such as the UCC28051, the switching currents and magnetics start to get "unreasonably" large > ~300W.  There are other factors that influence this such as the input voltage range the design has to operate over.

    Here is an example of a 350W reference design using the UCC28051 TM PFC controller: https://www.ti.com/tool/PMP22087 . I don't have any examples of a higher power design.

    It can be subjective as to what is "reasonable" or "unreasonable" since different applications have their key care-abouts.  However, somewhere around 200W - 300W, customers typically prefer either an interleaved solution such as the UCC28063/4A/5 family, so that the power is divided between the two phases (and therefore the power devices and magnetics can be sized accordingly), or a single-phase CCM controller such as the UCC28180 or UCC28019A.

    I hope this helps.

    Regards,

    Ray