Hi team,
I'd like to know about Reverse Protection.
Does this function mean that when EN is enabled and the input voltage is above 3.9V, the FET will turn off if VS is below 2.1V (TYP)?
In other words, even if EN is enabled, if a reverse voltage to VIN from VOUT is detected, the FET will turn off?
And, if EN is connected to VS, is it possible to configure reverse protection with one FET as follows?
Sincerely.
Kengo.