This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25071-Q1: OVP Threshold vs Temperature

Part Number: BQ25071-Q1
Other Parts Discussed in Thread: BQ25071

Figure 4. The OVP Threshold vs Temperature curve is slightly different. Why is it different between bq25071 and bq25071-Q1?

<BQ25071>


<BQ25071-Q1>

Regards,
Kagawa

  • Hello Kagawa

    I am looking into this question and will reply later tonight.

  • Hello Kagawa

    Recommend taking a look at our newer LiFePO4 charger BQ24171-Q1.  The charging profile for this device is friendlier to current generation of batteries.

    The Input over-voltage protection threshold is typically 10.5V with min of 10.2V and max of 10.8V. for both devices.   The two graphs show devices meeting this specification.

    Slight differences from device to device can be expected due to manufacturing variations.