This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Which simple switcher are pin + package compatible with the LMR14020 and functionally (nearly) compatible? (Not the LMR14030, other families...)
For the new application we have to show alternative simple switcher (pin + package + nearly functional compatible) for the LMR14020 to our customer.
Hi,
If i understand correctly, you have already identified LMR14030 and LMR14050 as pin to pin compatible part.
Another pin to pin compatible part would be LMR16020 and LMR16030 but they are a 60V part vs 40V part.
https://www.ti.com/product/LMR16020
Thanks
-Arief
One feature ist very important, the soft start time by power up.
We need a soft start time with max 1500 µs. It can be fix or adjustable - but max 1500 µs, better 1000 µs.
The LM14020 has an "External Soft-start", adjustable by a capacitor.
Important information to our requirement.
A delay between the input voltage and the output voltage is okay and uncritical.
Important is the "output ramp up time" - max 1500 µs are allowed from 0 V to 3,3 V at the output.
Hi Michi,
I apologize but i dont understand the question. Are you looking for a pin to pin compatible part with LMR14020 with adjustable soft-start time or are you looking for a part that have a soft-start at 1000us?
Thanks
-Arief
I'm looking for a pin to pin compatible part with LMR14020 with adjustable soft-start time.
How about LMR16030 which have the PGOOD and soft-start version
https://www.ti.com/lit/ds/symlink/lmr16030.pdf?ts=1644450784008&ref_url=https%253A%252F%252Fwww.google.com%252F#:~:text=The%20LMR16030%20is%20a%2060,power%20conditioning%20from%20unregulated%20sources.
Thanks
-Arief
The LMR16030 with soft start option looks good, seems to be a replacement for the LMR14020.
Are there any other possible switcher parts for the LMR14020?
We should have at least two other possible replacement families.