BQ27500DRZT-v130
- I need to understand how the BQ27500-v130 and BQ2057 play together in our design. Currently, we are using a dumb battery with an external NTC to control charging over temperature. The fuel gauge wants a thermistor input as well but I don’t think we want to parallel the charger and fuel gauge on one thermistor. We can’t rely on the processor to disable the charger at high/low temp because the device needs to charge when the processor is off. Can the temp input on the fuel gauge be unused?
-Is an eval available, I see the BQ27500EVM, is there an EVM for the BQ27500-V130?
-Tom-