This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM8A29: Drop-Out performance ?

Part Number: TPSM8A29

What is the drop out voltage operating down to 4.5V input at 12A & 15A load ?

Or is there a spec for R-drop out max ?  The DS efficiency figures at Vin = 5V stop for for a Vout = 2.5V, then switch to Vin =8V for Vout =3.3V.

Its not clear from the existing spec what can be output max setting in the low end operational Vin range ?