I'm trying to build as energy efficient a system as possible--for 12 to ~30V source voltage operation. I'd like to be able to use a supercap to provide a voltage for a time after power is lost...
Is it reasonable to use a supercap (say, for example, .25F) directly on the output rail of the TPS54260?
Do I need to use the SS/TR pin to limit current at startup?
Are there any other concerns with using the supercap as the output capacitor of the TPS54260?
Thanks!