The input capacitor and output capacitor of TPS73133DBV have a larger capacity than specified. (Specified 0.1 to 1uF, actually 47uF ceramic) Is there any problem in operation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The input capacitor and output capacitor of TPS73133DBV have a larger capacity than specified. (Specified 0.1 to 1uF, actually 47uF ceramic) Is there any problem in operation?
Hello,
Using a larger input capacitor will help improve line transient response. A larger output capacitor will help improve PSRR and load transient response. However, a serious drawback of increasing Output capacitance is that the inrush current during startup would dramatically increase. Its possible for the device to hit current limit (even thermal shutdown) during startup itself if the startup inrush current is large. Although not required for stability, we recommend that 1uF capacitors be used to attain the above mentioned benefits. Thanks!
Regards,
Srikanth