This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659039-Q1: PS659039,no PCM output found

Part Number: TPS659039-Q1


After debugging tps659039, it was found that PCM did not output. After checking, the power supply 5V and 3.3V were normal. The control signals given by the software include reset and EN,And also measured that the signal level is normal. Is there any signal that needs to be given? Can you help analyze it