Other Parts Discussed in Thread: UCC28951, UCC28950
I am testing a board (3.6KW Phase shifted full bridge DC-DC converter) which is using UCC28951QPWRQ1 controller. I am facing a problem which is that the IC is drawing about 250mA of current at VDD and the voltage at VDD is 9V instead of the 12V that I have on the board.I wanted to know what could make the IC draw all this current and why the voltage at VDD becomes 9V instead of 12V.