This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck-Boost product recommend

Dear team,

Could you please recommend TI Buck-Boost solution meet customer need:

adapter at least 300W

Input voltage: 9-36V 

Output voltage: 7~20V

Out current: 22A

Appreciate for your support and reply~

  • Hello Shuai,

    That's a very large range for Vin and Vout.

    I found a reference design for for a 4-switch buck-boost that is very close to those requirements:  PMP21278.

    Vin = 9V to 50V, Vout = 12V, Iout = 25A.

    There is also a design for USB-C at 20V/5A/100W:  PMP10698.  Perhaps the design could be modified with higher power output components to deliver 300W.

    Vin = 9V to 42V, Vout = 20V, Iout = 5A.

    Regards,

    Eric