Hi,
I take the low cost configuration design of LM2695 as reference for my application board, (Vin = 24V /Vout=10 Iout= 1.2 A same one in AN-1444 ). After first plug-in Vin=24VDC all good and (the consumption of my board 40mA in standby, then after 2-3 reset or plug-out and plug-in Vin, LM2695 is broken, I checked my design many times my deign all is ok, for the BOM, there is one modification the voltage divider on FB is 3K/1K, and the capacitor on output is low ESR same value 22uF, and I added a ressitor 2.2 ohms in serail, L=100uH/2A , and Diode Schottky 60V/2A.
But, I read again the datasheet, it is noted the capacitors C3 and C4 must be low ESR and C5 is recommended low ESR, but in my design they are not low ESR.
So my question if I change these capacitors (C3 = pin VCC, C4 = pin BST and C5 = Pin Vin) with other ones the same values and low ESR, could I fix this problem? for the capacitor C6=pin SS it isn't mandory to be low ESR?
BR
HA