This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23881: Using our custom TPS23881 board with the TPS2373-4EVM, cannot deliver more than 50W

Part Number: TPS23881

Hi there,

We have developed a custom PSE board using the TPS23811. The schematic is fairly vanilla, below is a screenshot, along with the key points:

  • Number of ethernet ports: 4
  • Onboard microcontroller: No
  • Configuration: Auto mode

We're aiming for this design to be able to work with any combination of different types of PoE devices connected. For example, a 2-pair 15W device on one port and a 4-pair 90W device on another port (or any other combination).

So far I'm testing this setup with the TPS2373-4EVM (PD eval board). I connect the TPS2373-4EVM to our custom board with a short RJ-45 cable and then simply change the jumpers (J7 and J10 set the PD type/class on the evm) on the TPS2372-EVM to configure it as different types of PD for testing.

I use an electronic load on the TPS2372-EVM to draw different power levels from it, while it is powered by our PSE board (using the TPS23811). Below is a diagram.

I'm able to verify it works for 40W delivered at the PD, 50W coming from PSE. However I can't seem to draw any more than that before the PSE shuts off power to the PD. I know the PD eval board is qualified to draw up to 90W from the PSE (71W at the PD), and I've checked all jumper settings.

So my question is, does the TPS23811 require anything else to be able supply 90W to a PD? I haven't changed anything on the SRAM, or have I written to any of the registers. Is this expected?

Thanks!