Customer wants to use TPS61062 EN pin for PWM dimming,datasheet indicates PWM should be less than 1kHz?I want to know why?I think,if I pull EN pin high at leat 1ms for the first time start up,we can improve PWM frquency 5KHz or 10KHz?According to TPS61062 block diagram,when TPS61062 starts up,EN pin is to shut off TPS61062 output by OVP circuit,I think 5K or 10K is ok for OVP circuit.