This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21710: Safety Input, output

Part Number: UCC21710
Other Parts Discussed in Thread: UCC21732

Hi Team,

I have question about the safety input.

What's the Ps means and how to deal with this specification?

According to the datasheet, the Ps is 1220mW maximum. but if I calcluate the value, the result should be as below.

68.3(℃/W)*1.22(W) = 83.33℃ ≠ 125(150 - 25)

it seems like that the specification has too margin. I want to understand how to design the thermal related.

Could you also tell me the differences between the Rthja and Figure 3 which is thermal derating curve for limiting power per VDE?

when I calculated the thermal resistance using the figure 3, the calclation result should be as below.

(150-25)℃/1.22W = 102℃/W

I think it's also gap between it and Rthja=68.3C/W. we want to know how to use the figure 3.

Regards,

Masa