This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLVH431A: ΔVref / ΔVka actual value

Part Number: TLVH431A


ΔVref / ΔVka described in the data sheet 6P is described as TYP = -1.5mV / V, but in Fig7 described in 9P, it is approximately -0.55mV / V (Ta = 25 ° C).
How much is your ability value?
If there is a variation distribution such as inspection data, please show it.

background
When designing with ΔVref / ΔVka = -1.5mV / V, the design value and the measured value do not match.
The actual value on hand is about -0.7mV / V.

  • Hi,

    The EC table does not have a minimum for this device so your testing is valid.

    Due do the age of the device, I do not have the distribution that was used for characterization to share.

    Is there a certain % of accuracy you are trying to achieve with this device?