Other Parts Discussed in Thread: TPS2115, TPS2113A, TPS2113,
Hi all,
I am considering using two TPS2116 in series to create a switching mechanism between 3 power supplies. I want to switch between a barrel jack, USB and a off board header, with priority given to the barrel jack, followed by the USB followed by the header.
I've been simulating the TPS2116 with the following circuit in PSpice with TI:
I am using the 5.1v on Vin2 simply to see which supply is being used but in reality both supplies should be 5V. As I understand, when PR1 drops below 1V, the supply will switch to Vin2, which it does. However it seems that as soon as Vin1 drops below 1V, thus meaning "MODE" is below 1V, the Vout goes to 0V. Please see the graph below. I have tied MODE to Vin1 for priority mode as instructed in section 7.6.1 of the datasheet which says:
"When MODE is tied high, PR1 determines the channel selected. To configure VIN1 as the priority supply, connect MODE to VIN1 and set the proper threshold through a resistor divider from VIN1 to PR1."
Vin2 follows Vin1 (so Vin2 is ON when Vin2 while Vin1 is off). I also have tried it with Vin2 as a DC supply
Pulse on Vin1 and Vin2
Pulse on Vin1, DC on Vin2
Note that when I tie Mode to Vin2 pulled high constantly, the device switches between the supplies without an issue.
Q1: Is this behaviour expected or have I made a mistake or misunderstood the datasheet? - should Mode be constantly high for priority mode and not tied to Vin1?
Q2: Do you have recommendations for the circuit component values to reduce the dip in Vout at switch over ?
Q3: TPS2116 is out of stock at the main suppliers - Can you provide SPICE files for other devices such as the TPS2113A or the TPS2115?
Thanks,
Peter