Hi, In the next design I need to create quiet power for PCIe interfce in the SOC.
The requirements are as follows:
1st power
must be an LDO
Uin1 - switcher output , I can set voltage to whatever I need to lower LDO power
Uout1-0.75V
Iout1 -1.8A
feedback pin(s) needed
good accuracy (1% if possible incl load and line), fast transient good PSRR ( I wil use ferrite on Uin1 so no need for super low PSRR)
2nd power
must be an LDO
Uin2 - switcher output , I can set voltage to whatever I need to lower LDO power, can (must) be different than Uin1
Uout2-1.8V
Iout -0.8A
feedback pin(s) needed
good accuracy (1% if possible incl load and line), fast transient, good PSRR ( I wil use ferrite on Uin2 so no need for super low PSRR)
I would prefer same LDO for both cases to easy manufacturing / sourcing.
All help appreciated - thanks